DOCA0216EN-00

Trip Unit Identification Number

The identification number 0000PPYYWWDLxxxxLV8••••• is made up as follows:

  • Serial number of the MicroLogic B trip unit in the format:

    • 0000PP = 0000 + Plant Code (6 alphanumeric characters)

    • YY = Year of manufacture

    • WW = Week of manufacture

    • D = Day of the week of manufacture (Monday = 1)

    • L = Line or machine number (alphanumeric characters)

    • xxxx = Unique product number during the day D

  • Commercial reference of the MicroLogic B trip unit (8 alphanumeric characters): LV8•••••

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?