DOCA0144EN-15

Firmware Version 001.000.206

Bugs Fixed

  • Incorrect calculation for In value:

    • Value displayed was twice the expected value

    • Impacted only 3-pole MTZ3 circuit breakers with External Neutral Current Transformer (ENCT)

  • Unexpected trip due to ground-fault protection test function occurred without pushing test button:

    • If the value of the current power supply (CPS) mode was decreasing at a specific rate while the voltage power supply (VPS) was being powered up simultaneously

    • Impacted only MicroLogic  6.0 X control units with VPS voltage power supply module

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?