Updating Firmware of MicroLogic X Control Unit
Prerequisites
The prerequisites for updating MicroLogic X firmware are the following:
-
The latest version of EcoStruxure Power Commission software is downloaded and installed on the PC.
-
The PC is connected to a power supply. Standby mode is deactivated to avoid the possibility of interruption during the update.
-
The PC is connected to the mini USB port on the MicroLogic X control unit by using the USB cable with part number LV850067SP.
-
The MicroLogic X control unit is continuously powered during the firmware update.
-
When the control unit is not connected to other ULP modules, it is powered by the PC through the mini USB port.
-
When the control unit is connected to other ULP modules, it is powered by an external 24 Vdc power supply.
-
For more information, refer to EcoStruxure Power Commission Online Help.
Procedure for Updating MicroLogic X Firmware
| NOTICE |
|---|
|
HAZARD OF INTERRUPTION OF POWER SUPPLY
Failure to follow these instructions can result in deterioration
of the control unit.
|
During the firmware update, the standard protection functions of the MicroLogic X control unit are operational. No data or measurements are available or refreshed on the different communication interfaces.
Follow this procedure to update the firmware version of the MicroLogic X control unit:
| Step | Action |
|---|---|
| 1 | Disable all wireless access (Bluetooth and NFC) between the MicroLogic X control unit and a smartphone. |
| 2 | Use the USB cable with part number LV850067SP to connect a PC to the mini USB port on the front face of the MicroLogic X control unit. |
| 3 | |
| 4 | |
| 5 | |
| 6 | |
| 7 | Go to the Configure section and click Write to Project to save the MicroLogic X settings. |
| 8 | Click Firmware. |
| 9 | |
| 10 | |
| 11 | |
| 12 |
EcoStruxure Power Commission software displays the following message during an update: The update takes approximately 10 minutes. NOTE: Do not connect a smartphone to the MicroLogic X control unit during the firmware update. NOTE: During the firmware update, the standard protection functions of the MicroLogic X control unit are operational. No data or measurements are available or refreshed on the different communication interfaces. The MicroLogic X control unit screen displays the following message during an update: |
| 13 |
When the update is finished, EcoStruxure Power Commission software displays a message indicating that the device has been successfully updated. Click CLOSE to acknowledge. |
| 14 |
Result: EcoStruxure Power Commission software indicates other Enerlin’X devices which need to be updated, if any. If the page does not refresh automatically, click REFRESH. The status indicates whether the firmware of other modules is compatible with the firmware version of the MicroLogic control unit:
|
| 15 | Update the firmware version of associated Enerlin’X devices, if any (see Updating Firmware of Enerlin’X Devices). |
NOTE: When updating aMicroLogic X control unit with firmware version 001.000.200 to the latest version of the firmware, red pop-up trip or alarm messages may be displayed on the MicroLogic X display screen following the firmware update. This corresponds to trip or alarm messages that were not acknowledged by the user before the firmware update. Press the ESC button on the control unit to remove these messages.