DOCA0144EN-15

Firmware Version 002.000.004

Bugs Fixed

  • High consumption of battery in specific cases without auxiliary power supply

  • The following alarms and pop-up messages were generated spuriously on display screen of MicroLogic X control unit:

    • Protection settings reset to factory value (0x1430)

    • Error 21 – Service not performed – Internal error

    • Error 190 –  Service not performed – Internal error

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?