Purchasing and Installing a Digital Module
Prerequisites
The prerequisites to purchasing and downloading a Digital Module are as follows:
-
The firmware version of the MicroLogic X control unit must be compatible with the Digital Module (refer to table below). Update the firmware version of the MicroLogic X control unit if the Digital Module required is not compatible.
| Digital Module | Commercial reference | Minimum MicroLogic X firmware version |
|---|---|---|
|
ANSI 51G - IDMT ground-fault protection |
LV850038 |
005.103.003 |
| IEC 61850 for MasterPact MTZ | LV850046 | 004.101.000 |
| ANSI 67 - Directional short-time overcurrent protection | LV850015 | 004.101.000 |
| ANSI 51 - IDMTL overcurrent protection | LV850037 | 004.101.000 |
| ANSI 81 - Under/Over frequency protection | LV850013 | 003.012.000 |
| Individual harmonics analysis | LV850006 | 002.000.002 |
| ANSI 27/59 - Under/Over voltage protection | LV850012 | 002.000.002 |
| ANSI 32P - Reverse active power protection | LV850011 | 002.000.002 |
| ANSI 51N/51G - Ground-fault alarm | LV850007 | 002.000.002 |
| Energy Reduction Maintenance Settings (ERMS) | LV850009 | 002.000.002 |
| Modbus legacy dataset | LV850045 | 002.000.002 |
| Energy per phase | LV850002 | 001.000.002 |
| Power restoration assistant | LV850004 | 001.000.002 |
| MasterPact operation assistant | LV850005 | 001.000.002 |
| Waveform capture on trip event | LV850003 | 001.000.002 |
-
The latest version of EcoStruxure Power Commission software is downloaded and installed on the PC.
-
The PC is connected to a power supply.
-
The PC is connected to the Internet.
-
You have the identification number of the MicroLogic X control unit.
-
You have the commercial reference of the Digital Module to be purchased.
-
You provide the email address to receive the Installer email containing Digital Module download information.
Getting Control Unit Identification Number
You can get the control unit identification number on site or off site using one of the following means:
-
On site, by scanning the QR code on the front face of the MicroLogic X control unit from a smartphone. The QR code identifies the MicroLogic X control unit. Use the Share button to share the control unit information with the person qualified to select and purchase Digital Modules.
-
On site, from EcoStruxure Power Commission software with a PC connected to the mini USB port of the MicroLogic X control unit.
-
Off site, from EcoStruxure Power Commission software. This access can only be used for a MicroLogic X control unit previously registered in the relevant project.
Purchasing and Downloading a Digital Module
Follow this procedure to purchase and download a Digital Module:
| Step | Action |
|---|---|
|
1 |
Contact your local Schneider Electric Customer Care Center (CCC) or Schneider Electric Services Representative. Visit the www.se.com website to contact your local Schneider Electric CCC. |
|
2 |
Provide the information indicated in Prerequisites and purchase the Digital Module. You will receive an Installer email at the address you indicated to CCC. |
|
3 |
Select the email from dsc-no-reply@verified.se.com to download your Digital Module. The subject is Your Digital Modules are ready for download. Your Digital Module appears in a list of items ready to be downloaded. NOTE: If you do not see the email
in your Inbox, check the Junk mailbox.
|
|
4 |
Click the checkbox next to the Digital Module that you want to download and click Download to download the delivery package. NOTE: This delivery package is used to install the Digital Module on the MicroLogic X
control unit using EcoStruxure Power
Commission
software. Make sure that the delivery
package is present on the PC used to install a Digital Module.
NOTE: If the Digital
Module was purchased previously, you can access the file downloaded
by clicking the following link: https://digitalpackage.schneider-electric.com/dpb?lang=en.
|
Installing a Digital Module on the MicroLogic X Control Unit
The MicroLogic X Administrator, Services, or Engineer password is required to install a Digital Module on the MicroLogic X control unit.
Follow this procedure to install a purchased Digital Module on a MicroLogic X control unit.
| Step | Action |
|---|---|
| 1 | Use the USB cable with part number LV850067SP to connect a PC running EcoStruxure Power Commission software to the mini USB port on the front face of the MicroLogic X control unit. |
| 2 |
Click Connect to device directly to establish a connection between the EcoStruxure Power Commission software and the MicroLogic X control unit. EcoStruxure Power Commission software displays the MicroLogic X control unit identification number on the screen. |
| 3 |
Open the Digital Module page by clicking Digital Modules. |
| 4 |
Check that the delivery package for the Digital Module to be installed is present on the PC being used. |
| 5 |
Select the Digital Module to be installed by clicking Install. The standard protection functions of the MicroLogic X control unit remain active during installation of the Digital Module. NOTE: Only modules
previously purchased can be installed directly by clicking Install.
|
| 6 |
EcoStruxure Power Commission software asks you to confirm the installation. Enter the Administrator password and click CONTINUE. |
| 7 | |
| 8 |
When installation is complete and before unplugging the PC, disconnect EcoStruxure Power Commission software from the MicroLogic X control unit by clicking the Disconnect button. |
| 9 |
Use the EcoStruxure Power Device app to check that the Digital Module is installed. |
| 10 |
Use the EcoStruxure Power Device app or EcoStruxure Power Commission software to check that the Digital Module is working correctly. |
For more information, refer to EcoStruxure Power Commission Online Help .
NOTE: To uninstall a Digital Module, use EcoStruxure Power Commission software.