DOCA0144EN-15

Firmware Version 005.103.003

New Features

  • Compatibility with the ANSI 51G - IDMT ground-fault protection optional Digital Module.

  • Digital Modules are available to purchase and install by contacting Schneider Electric Customer Care Centre or Schneider Electric Services.

    NOTE: The Schneider Electric GoDigital marketplace is no longer available.

Bugs Fixed

  • Firmware update process was stuck when MicroLogic X control unit was in non-nominal state.

  • The event Invalid Bluetooth communication (0x1422) was generated spuriously.

  • The MicroLogic X display screen was rebooting spuriously.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?