DOCA0144EN-15

Firmware Version 004.107.000

New Features

  • Performance improvement of self-test to monitor the presence of internal current power supply (CPS) sensors

    NOTE: The discontinuity of internal current power supply (CPS) sensor can lead to user exposure to electric hazard. As a default behavior, a failed self-test can result in the opening of the circuit breaker to help to ensure user and material protection. In this case, the trip message Replace Circuit Breaker Self Diagnostic (0x641F) will be generated. For more information about this behavior, contact your Schneider Electric Customer Care Center and mention the following reference: FAQ000190726.

  • Addition of automatic acknowledgment mode for orange pop-up messages related to medium severity protection alarms on the MicroLogic display screen

Bugs Fixed

  • The event Last protection settings have not been applied (0x142F) was generated spuriously.

  • The event Schedule manufacturer maintenance within three months (0x1482) was generated prematurely due to absence of commissioning date entered by the user in EcoStruxure Power Commission software.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?