DOCA0144EN-15

Firmware Version 003.011.000

New Features

  • Addition of maintenance schedule reminder events to help user to plan preventive maintenance programs

  • Password management: enhancement of user profiles from levels to role profiles

  • Addition of ERMS force unlock command to unlock ERMS function if smartphone used to engage the function is unavailable

Bugs Fixed

  • Possible loss of voltage release configuration

  • The following events were generated spuriously:

    • Control unit self test #5 (0x1473)

    • Earth leakage (Vigi) sensor disconnected (0x1408)

    • Invalid Control Unit factory config #1 (0x0D0A)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?