DOCA0144EN-15

Firmware Version 002.000.003

New Features

Conformity to UL/ANSI standard with the addition of the following control units:

  • MicroLogic  3.0 X control unit (LV848815)

  • MicroLogic  5.0 X control unit (LV847609)

  • MicroLogic  6.0 X control unit (LV847608)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?