DOCA0144EN-15

Firmware Version 002.000.002

New Features

  • Compatibility with the following optional Digital Modules (available through the Schneider Electric GoDigital marketplace):

    • ANSI 27/59 - Under/Over Voltage Protection Digital Module

    • ANSI 32P - Reverse Active Power Digital Module

    • ANSI 51N/51G - Ground-Fault Alarm Digital Module

    • Individual Harmonics Analysis Digital Module

    • Modbus Legacy Dataset Digital Module

    • Energy Reduction Maintenance Settings (ERMS) Digital Module

  • Addition of support for ERMS switch module (ESM)

  • Protection setting procedure in 2 steps (Submit/Apply) for compliance with UL489SE

  • Addition of current and power demand

  • New calculation method for minimum and maximum values for current, voltage, and power factor

  • Addition of load profile monitoring

  • Multiple events assignment with M2C or IO module

  • Addition of long waveform capture in the Waveform Capture on Trip Event Digital Module

  • Additional information with Configuration mismatch between IO and control unit event message

  • Enhancement of reliability of event management and time-stamping

  • Addition of event code on event messages to improve diagnosis

  • Enhancement of internal battery test pattern

  • Enhancement of internal battery loss management

  • Enhancement of external 24 Vdc power supply management

  • Improved robustness of the file system management

Bugs Fixed

  • Bluetooth LED remained on with Error 5 displayed, requiring control unit to be switched off and on

  • Snapshot was not showing correct Ii coefficient pickup when Instantaneous protection was set to OFF

  • Frequency measurement was shifted and/or unstable in 3-pole system using 3-wattmeter calculation

  • Loss of event message Configuration mismatch between IO and control unit occurred when power cycling the control unit

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?