Introduction
MicroLogic X Control Unit
MasterPact MTZ circuit breakers with MicroLogic X control units provide protection functions, metering, diagnostics, communication, and remote operations.
The control unit is customizable with optional Digital Modules.
MicroLogic X control units allow operation and monitoring of MasterPact MTZ circuit breakers locally or remotely.
MicroLogic X Firmware Release History
| Date | MicroLogic X Firmware version | Availability |
|---|---|---|
|
February 2024 |
005.103.003 |
Release for manufacturing |
|
February 2023 |
005.103.003 |
Digital release in EcoStruxure Power Commission (EPC) software |
|
October 2021 |
004.109.000 |
Obsolete |
|
March 2021 |
004.107.000 |
Obsolete |
|
October 2020 |
004.105.003 |
Obsolete |
|
April 2020 |
004.105.000 |
Obsolete |
|
December 2019 |
004.101.000 |
Obsolete |
|
July 2019 |
003.012.000 |
Obsolete |
|
March 2019 |
003.011.000 |
Obsolete |
|
November 2018 |
002.000.004 |
Obsolete |
|
April 2018 |
002.000.003 |
Obsolete |
|
March 2018 |
002.000.002 |
Obsolete |
|
December 2017 |
001.000.206 |
Obsolete |
|
July 2017 |
001.000.202 |
Obsolete |
|
December 2016 |
001.000.200 |
Obsolete |
Firmware Update Policy
If the latest features of a firmware update are not required, it is not mandatory to update the firmware of a device.
Use this document to determine whether an update to the latest version of the MicroLogic X firmware is interesting or relevant for your application.
For more information about the firmware update policy and the firmware compatibility between devices, refer to DOCA0155EN MicroLogic Trip Units and Control Units - Firmware History .
Firmware Update with EcoStruxure Power Commission Software
EcoStruxureTM Power Commission is the new name of Ecoreach software.
Use the latest version of EcoStruxureTM Power Commission software:
-
To check the firmware compatibility of the devices in the IMU
-
To update the devices with the latest firmware version available
After updating the firmware of one device, use EcoStruxure Power Commission software to check the firmware compatibility between IMU devices.
The Firmware Update table helps you to diagnose and identify all discrepancy issues between IMU devices. This table also provides the recommended actions for each discrepancy issue.
The latest version of EcoStruxure Power Commission software is available at: www.se.com.
For more information about the use of EcoStruxure Power Commission software, refer to EcoStruxure Power Commission Online Help.