DOCA0144EN-15

Firmware Version 004.101.000

New Features

  • Compatibility with the following optional Digital Modules (available through the Schneider Electric GoDigital marketplace):

    • ANSI 51 – IDMTL overcurrent protection

    • ANSI 67 – Directional overcurrent protection

    • IEC 61850 for MasterPact MTZ

  • Compatibility with communication features:

    • RSTP (Rapid Scanning Tree Protocol)

    • NTP (Network Time Protocol)

  • Addition of contact wear interpretation to facilitate the preventive maintenance of the circuit breaker

  • Firmware update process made faster and more reliable

Bugs Fixed

The following events were generated spuriously and simultaneously on display screen of MicroLogic X control unit:

  • Control unit self test #2 (0x1470)

  • Firmware Discrepancy within control unit (0x0D09)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?