DOCA0284EN-04

Final Checks and Reporting

This topic is present in MTZ1 and MTZ2-3 (Commissioning). Any changes made will be made in all these guides.

Final Checks

After completing the commissioning tests, check the following:

Step

Action

1

Check that connections are made with the correct tightening torque, that there are no tools or objects inside the equipment, and that all circuit breakers, doors, and protective covers are in position.

2

Check that the circuit breaker is open (OFF position) and the closing spring is charged.

Project Report Generated by EcoStruxure Power Commission Software

EcoStruxure Power Commission software generates a project report with a list of the circuit breakers for that project. For each MasterPacT MTZ circuit breaker it provides the following information:

  • The circuit breaker identification data

  • The MicroLogic Active identification data

  • The list of accessories including internal accessories and external modules

  • The protection settings for the MicroLogic Active control unit

  • The alarm settings

  • The IFE, EIFE or IFM communication interface settings

  • The BCIM module settings

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?