Tests
Overview
The tests to do while commissioning a MasterPacT MTZ circuit breaker are described in this section:
-
Functional checks
-
Check of MCH gear motor (if fitted)
-
Check of BCIM module (if fitted)
-
Check of electrical continuity
-
Check of high-voltage insulation
-
Check of MicroLogic Active internal battery
-
Check of MicroLogic Active Ready LED status
-
Test of the tripping mechanism on the MicroLogic Active display screen
-
Automatic trip curve test with EcoStruxure Power Commission software
Only do the tests required, depending on the MasterPacT MTZ type and the functions in use, and record the results on the test form. In the event of non-conformance, the result must be recorded and the MasterPacT MTZ circuit breaker must not be accepted into service.
Functional Checks
Follow this procedure to check the operation of the MasterPacT MTZ circuit breaker and record the results on the test form.
|
Step |
Action |
|---|---|
|
1 |
Manually charge the mechanism by pulling the spring charging handle down. |
|
2 |
Close the circuit breaker. Check the closing of the circuit breaker in each of the different means designed for the application. |
|
3 |
Open the circuit breaker. Check the opening of the circuit breaker in each of the different means designed for the application. |
If the circuit breaker does not close or does not open, refer to Troubleshooting.
Check of MCH Gear Motor (if Fitted)
Follow this procedure to check the operation of the MCH gear motor and record the results on the test form.
|
Step |
Action |
|---|---|
|
1 |
Remove the MCH gear motor power supply. |
|
2 |
Do an opening/closing/opening cycle to discharge the mechanism. |
|
3 |
With the circuit breaker in the open position and the mechanism discharged, check electrical continuity between terminals B1 and B2, and electrical non-continuity between terminals B1 and B3. |
|
4 |
Manually charge the mechanism. |
|
5 |
Reconnect the MCH gear motor power supply. The circuit breaker closes and the mechanism is automatically charged. |
|
6 |
Check electrical continuity between terminals B1 and B3. |
|
7 |
Operate the circuit breaker several times to check that the spring mechanism automatically recharges after every closing operation. |
Check of BCIM Module (if Fitted)
The checks performed on the BCIM module depend on the configuration which is used.
Follow this procedure when the BCIM module is present with the BCIM IO mode set to ERMS. Record the results on the test form.
|
Step |
Action |
|---|---|
|
1 |
Make sure the MicroLogic Active control unit and BCIM module are powered. |
|
2 |
Connect the BCIM IO channel used for ERMS engagement to an external selector switch. |
|
3 |
Select ERMS IO mode on the MicroLogic Active display screen at . |
|
4 |
Engage the ERMS function by turning the external selector switch. Check that:
|
|
5 |
Disengage the ERMS function by turning the external selector switch and check that the MicroLogic Active control unit returns to it’s original state. |
Follow this procedure when the BCIM module is present with the BCIM IO mode set to Open/Close. Record the results on the test form.
|
Step |
Action |
|---|---|
|
1 |
Close the circuit breaker. |
|
2 |
Make sure the MicroLogic Active control unit and BCIM module are powered. |
|
3 |
Connect the BCIM IO channels to external pushbuttons:
|
|
4 |
Select Open/Close IO mode on the MicroLogic Active display screen at . |
|
5 |
Open the circuit breaker by pressing the external pushbutton connected to BCIM IO channel 1. |
|
6 |
Check that the circuit breaker is open. |
|
7 |
Close the circuit breaker by pressing the external pushbutton connected to BCIM IO channel 2. |
|
8 |
Check that the circuit breaker is closed. |
Check of Electrical Continuity
Follow this procedure to check electrical continuity using a multimeter or continuity checker and record the results on the test form.
|
Step |
Action |
|---|---|
|
1 |
Close the circuit breaker. |
|
2 |
Check electrical continuity, for each of the phases, between the upper and lower power terminals:
|
Check of High-Voltage Insulation
Dielectric tests (high potential and insulation resistance tests) are used to check the insulation between phases, and insulation between each phase and ground. The equipment used to conduct these tests creates a high potential voltage (thousands of volts) to check dielectric or insulation integrity.
Before conducting any high-voltage insulation tests, unplug any cables from the USB-C port on the front face of the MicroLogic Active control unit.
Follow this procedure to check insulation resistance and record the results on the test form.
|
Step |
Action |
|---|---|
|
1 |
Unplug any cables from the USB-C port on the front face of the MicroLogic Active control unit. |
|
2 |
Close the MasterPacT MTZ circuit breaker. |
|
3 |
Measure the insulation resistance using a 500 Vdc insulation resistance tester between one of the phases and the other two phases grounded. Repeat for each phase. |
|
4 |
Open the MasterPacT MTZ circuit breaker by pressing the opening pushbutton. |
|
5 |
Measure the insulation resistance using a 500 Vdc insulation resistance tester between one of the phases and ground, with all other phases grounded. Repeat for each phase. |
|
6 |
Check that the insulation resistance is above 5 MΩ in each case. If this result is not obtained, contact your Schneider Electric Services representative. |
Check of MicroLogic Active Internal Battery
Follow this procedure to check the functioning of the MicroLogic Active internal battery.
|
Step |
Action |
|---|---|
|
1 |
Press and hold the |
|
2 |
Check that the trip cause LEDs switch off for one second, and then switch on. If the trip cause LEDs:
|
Check of MicroLogic Active Ready LED Status
Follow this procedure to check the functioning of the MicroLogic Active control unit and record the results on the test form.
|
Step |
Action |
|---|---|
|
1 |
Provide power to the MicroLogic Active control unit, for example, by connecting a PC or Mobile Power Pack to the USB-C port on the front face. |
|
2 |
Check that the MicroLogic Active Ready LED is flashing green. The Ready LED flashes green to indicate that:
|
|
3 |
If the Ready LED is not flashing green, refer to Critical Cases. |
Test of the Tripping Mechanism on the MicroLogic Active Display Screen
Follow this procedure to test the tripping mechanism of the circuit breaker and record the results on the test form.
Automatic Trip Curve Test With EcoStruxure Power Commission Software
Follow this procedure to run the automatic trip curve test and record the results on the test form.
|
Step |
Action |
|---|---|
|
1 |
Close the circuit breaker. |
|
2 |
If the circuit breaker is equipped with an MN undervoltage release, either connect it to the power supply with its rated voltage or remove the MN undervoltage release. |
|
3 |
Connect a PC running EcoStruxure Power Commission software by using a cable to the USB-C port on the front face of the MicroLogic Active control unit. |
|
4 |
On EcoStruxure Power Commission software, select the circuit breaker and connect to it. |
|
5 |
Select the Automatic Trip Test section. |
|
6 |
Select Preconfigured test point. |
|
7 |
Select the overcurrent protection to be tested. |
|
8 |
Click Run Test. |
|
9 |
Check that the circuit breaker trips. |
|
10 |
Check that the blue fault-trip reset button has popped out |
|
11 |
Check that the related trip cause LED is blinking red. |
|
12 |
Check the SDE contacts have switched. |
|
13 |
After the test, reset the circuit breaker. |