Circuit Breaker Identification
Identification
The MasterPacT MTZ1 circuit breaker can be identified in the following ways:
-
Rating plate on circuit breaker
-
QR code located on the front face of the control unit of the circuit breaker
-
Identification labels on the circuit breaker and on the chassis
Product Identification Label
|
Legend |
Description |
Explanation |
|---|---|---|
|
A |
Product code |
The product code is a line of code representing the complete configuration of a MasterPacT circuit breaker. It is automatically generated for each MasterPacT circuit breaker after completing the configuration by using the Product Selector configuration tool. The product code appears on the invoice and on the delivery documents as well as on the MasterPacT circuit breaker and packaging labels. The product code can be entered in the Product Selector configuration tool, which generates the complete configuration of the MasterPacT circuit breaker. |
|
B |
Schneider Electric internal identification numbers |
– |
|
C |
Description of circuit breaker |
The description of the circuit breaker, specifies the following characteristics:
|
|
D |
Certification logos |
The logos of the mandatory certifications of the circuit breaker. |
|
E |
Circuit breaker serial number |
The circuit breaker serial number is coded PPYYWWDNNNN, where:
For example, PP240730064 is the sixty-fourth circuit breaker manufactured at plant PP on Wednesday, February 14, 2024. |
Product Checked Label
|
Legend |
Description |
Explanation |
|---|---|---|
|
F |
Circuit breaker serial number |
See explanation in preceding table. |
|
G |
Circuit breaker test date code |
The circuit breaker test date code is coded PPYYWWD HH:MM, where:
|
Accessory Voltages Label
Rating Plate
The rating plate with the circuit breaker information is located on the front cover of the circuit breaker.
QR Code
When the QR code on the front face of a MasterPacT MTZ circuit breaker is scanned with a smartphone running a QR code reader and connected to the Internet, the Go2SE landing page is displayed.
The landing page displays:
-
Information about the MicroLogic Active control unit, including traceability information.
-
Zigbee ID and installation code for MicroLogic Active AP/EP control unit.
-
A list of menus.