DOCA0284EN-04

Drawout MasterPacT MTZ1 Circuit Breaker Status

@experts: Topic shared between DOCA0284 and DOCA0285, with profiling; indicate if comments do not apply to both guides

Drawout Circuit Breaker Handling Conditions

Connection or disconnection of the drawout circuit breaker requires insertion of the racking handle. When interlocks, padlocks, or an open door lock are in place, the racking handle cannot be inserted.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E or CSA Z462 or local equivalent.
  • This equipment must only be installed and serviced by qualified electrical personnel.
Failure to follow these instructions will result in death or serious injury.

Drawout Circuit Breaker Positions

The indicator located on the front of the chassis locally signals the position of the circuit breaker in the chassis.

Circuit breaker position

Position indicator and position contact state

Connector position

Circuit breaker status

Connected

  • Disconnecting contact clusters: engaged

  • Control: engaged

  • Can be operated.

  • Ready for service.

Test

  • Disconnecting contact clusters: disengaged - the minimum distance between the circuit breaker racking terminals and the chassis clusters is reached.

  • Control: engaged

  • Can be operated.

  • Can have operation and control systems tested.

Disconnected

  • Disconnecting contact clusters: disengaged

  • Control: disengaged

  • Can be operated.

  • Can be removed from chassis.

Withdrawn

  • Disconnecting contact clusters: disengaged

  • Control: disengaged

Removed from chassis.

Drawout Circuit Breaker Position Contacts

The position of the circuit breaker in the chassis is indicated remotely by the following position contacts:

  • CE: connected position

  • CT: test position

  • CD: disconnected position

The state of the position contacts changes according to the circuit breaker position during racking-in and racking-out operations, as shown in the diagram below.

A Circuit breaker in connected position

B Separation of the main circuits

C Circuit breaker in test position

D Separation of auxiliary circuits

E Circuit breaker in disconnected position

Position contact is open.

Position contact is closed.

Drawout Device Position Contacts Without EIFE Ethernet Interface

Without EIFE Ethernet interface, optional position contacts can be added as follows:

  • 2 CD disconnected position contacts

  • 3 CE connected position contacts

  • 1 CT test position contact

Drawout Device Position Contacts With EIFE Ethernet Interface

With EIFE Ethernet interface, 2 optional CE connected position contacts can be added.

Chassis Management Function

The chassis management function is used to:

  • Record and check the position of the moving part of the drawout device in the chassis

  • Provide information about preventive maintenance actions

  • Notify the remote controller about the position of the drawout device

The chassis management function is performed by the EIFE Ethernet interface. Refer to DOCA0106•• Enerlin'X EIFE - Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker - User Guide in Related Documents at the beginning of this guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?