DOCA0284EN-04

Drawout Circuit Breaker

@experts: Topic shared between DOCA0284 and DOCA0285, with profiling; indicate if comments do not apply to both guides

Definition

A drawout circuit breaker is composed of the moving part (also called the circuit breaker) and the fixed part (or chassis).

Drawout Circuit Breaker Moving Part Description

The following image shows the standard version of the moving part of a drawout circuit breaker (no optional accessories).

A Carrying grip

B Arc chute

C Product identification label, with manufacturing date

D Blue fault-trip reset button

E Opening pushbutton

F Closing pushbutton

G Disconnectable contact block cover

H Front cover

I Spring charging handle

J VBP pushbutton locking cover (optional)

K Rating plate

L Spring charged and ready-to-close indicator

M Main-contact position indicator

N Window to consult the (optional) CDM mechanical operation counter

O Control unit

P Control unit transparent cover

Drawout Circuit Breaker Accessories Description

The following image shows the accessories available for the moving part of a drawout circuit breaker.

A VDC mismatch protection

B Disconnectable contact block

C Four OF indication contacts (delivered as standard)

D MCH gear motor

E CDM mechanical operation counter

Z1, Z2 See following images

The following images zoom in on the accessories for the moving part of a drawout circuit breaker.

F Standard SDE1 fault-trip indication contact

G Optional SDE2 fault-trip indication contact or RES electrical remote reset

H Microswitch

I BCIM module

J MN undervoltage release or MX2 opening voltage release

K XF closing voltage release

L MX1 opening voltage release

M PF ready-to-close contact

N VSPO OFF-position locking by keylocks

O VCPO OFF-position locking by padlocks

Chassis Description

The following image shows the standard version of the chassis (no optional accessories).

A Carrying grip

B Terminal blocks for standard accessories

C Terminal block identification plate

D Chassis locking by padlocks

E Moving part position indicator

F Racking handle socket

G Position release button

H Racking handle storage space

I Racking handle

J Drawout grip

K Extension rail

L Top safety shutter

M Bottom safety shutter

Chassis Accessories Description

The following image shows the accessories available for the chassis.

A VDC mismatch protection

B Drawout device position contacts

C Terminal blocks for optional accessories

D ULP cord

E EIFE embedded Ethernet interface

F VSPD chassis locking by keylocks

G VPOC open-door racking interlock

H Circuit breaker auxiliary terminal shield

I VPEC door interlock

Chassis Terminal Block Description

Terminal block supplied as standard on the chassis

Optional terminal block on the chassis

NOTE: Two markings are possible for the COM and UC3 terminal blocks.
 

Old marking

New marking

 

Assignment of Chassis Terminal Blocks

DANGER
HAZARD OF ELECTROCUTION FOR VOLTAGES ABOVE 480 VAC
If a voltage greater than 480 Vac is connected to a terminal, it is forbidden to connect adjacent terminals to a 24 Vdc SELV (Safety Extra Low Voltage) power supply in order to observe the insulation distances. For example, if you connect a 690 Vac supply to the UC4 terminal block, you must not connect a 24 Vdc SELV supply to the SDE2 terminal block.
Failure to follow these instructions will result in death or serious injury.

The following table describes the assignment and the availability of the terminal blocks for drawout circuit breakers:

  • Standard terminal blocks are delivered on the chassis, even if the associated accessories are not installed in the circuit breaker.

  • Optional terminal blocks are delivered on the chassis only if the associated optional accessories are installed in the circuit breaker.

Block

Marking

Description

Availability

A

CE2-CE3

2 CE connected position contacts

Optional

B

COM

MicroLogic Active without BCIM module:

  • Terminal block for the external power supply of the MicroLogic Active control unit

Standard

MicroLogic Active with BCIM module:

  • Terminal block for the connection of the BCIM module to ULP modules, by using the circuit breaker ULP cord

  • or ULP port module for the connection of the BCIM module to ULP modules, by using a ULP cord

Optional

UC1

Zone selective interlocking (ZSI)

Standard

UC2

Neutral external sensor

Standard

SDE2/RES

SDE2 additional fault-trip indication contact or RES electrical remote reset

Optional

M2C/UC4/ESM

MicroLogic Active without BCIM module:

  • External phase voltage

MicroLogic Active with BCIM module:

  • External phase voltage

  • or 2 BCIM IO channels

Optional

UC3

MicroLogic Active without BCIM module:

  • External neutral voltage

MicroLogic Active with BCIM module:

  • External neutral voltage and external power supply of the MicroLogic Active control unit

Standard on 3P circuit breakers

Optional on 4P circuit breakers

SDE1

SDE1 fault-trip indication contact

Standard

MN/MX2

MN undervoltage release or MX2 opening voltage release

Standard

MX1

MX1 opening voltage release

Standard

XF

XF closing voltage release

Standard

PF

PF ready-to-close contact

Standard

MCH

MCH gear motor

Standard

OF1-OF4

4 OF indication contacts

Standard

C (without EIFE interface)

CD1-CD2

2 CD disconnected position contacts

Optional

CE1

1 CE connected position contact

CT1

1 CT test position contact

C (with EIFE interface)

EIFE

EIFE embedded Ethernet interface

Optional

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.