DOCA0284EN-04

Zigbee Wireless Communication Commissioning

@TW: topic shared between DOCA0284 and DOCA0285

MicroLogic Active AP/EP Control Unit Discovery with Panel Server

The prerequisites to discovering a MicroLogic Active AP/EP control unit with a Panel Server are:

  • The control unit must be a MicroLogic Active AP/EP control unit.

  • The Panel Server must be turned on.

  • The MicroLogic Active AP/EP control unit and Panel Server must be in close proximity.

It is recommended to perform the commissioning of Zigbee wireless devices in a place secure from rogue radio transmitters, such as an administrator room. For more information, refer to DOCA0122•• MasterPacT, ComPacT, PowerPacT - Cybersecurity Guide in Related Documents at the beginning of this guide.

Follow the procedure below to discover a MicroLogic Active AP/EP control unit with a Panel Server:

Step

Action

1

Turn on the Panel Server.

2

Follow the discovery procedure described in EcoStruxure Panel Server - User Guide in Related Documents, at the beginning of this guide.

3

When prompted to do so, connect the MicroLogic Active AP/EP control unit to a Zigbee network.

Do this by selecting Connect on the MicroLogic Active display screen, from the tree navigation menu, at Configuration > Communication > IEEE 802.15.4 > Status.

4

At the end of the discovery procedure, the MasterPacT MTZ circuit breaker with MicroLogic Active AP/EP control unit appears in the list of discovered devices on Panel Server webpages.

NOTE: It is recommended that the MicroLogic Active AP/EP control unit is powered by an external 24 Vdc power supply, to avoid communication loss if the load falls below 20% of the rated current In.

Zigbee Wireless Communication Discovery Video

To access a demonstration video about discovery of the MicroLogic Active AP/EP control unit with Panel Server, click here, scan the QR code, or copy and paste the link to your Web browser:

Zigbee Wireless Communication Test

After discovery of the MasterPacT MTZ circuit breaker with MicroLogic Active AP/EP control unit, you can check Zigbee wireless communication and microswitch installation.

Step

Action

1

Select the Monitoring & Control menu on Panel Server webpages.

2

Select the MasterPacT MTZ circuit breaker with MicroLogic Active AP/EP control unit to test, from the list of discovered devices.

3

Check the circuit breaker status.

4

If the circuit breaker status (open or closed), displayed on Panel Server webpages does not match the actual status of the circuit breaker, contact your Schneider Electric Services representative.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?