DOCA0284EN-04

Circuit Breaker Interlocking Actions

@experts: Topic shared between DOCA0284 and DOCA0285, with profiling; indicate if comments do not apply to both guides

About Interlocking Actions

An interlocking action is an automatic locking operation provided by interlocking accessories added to the MasterPacT MTZ1 circuit breaker or chassis.

A number of optional interlocking accessories are available for the MasterPacT MTZ1 circuit breaker and chassis. For a complete listing of available interlocks, refer to LVPED225010EN MasterPacT MTZ with MicroLogic Active Control Unit - Catalog in Related Documentsat the beginning of this guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?