Chassis Locking in Any Position
Description
The chassis can be locked in any position (connected, test, or disconnected position).
This locking function requires a mechanical adaptation of the chassis, explained in the following procedure.
When the chassis is locked, the racking handle cannot be inserted in the racking handle socket.
The chassis can be locked in any position:
-
By up to three padlocks with shackle diameter 5-8 mm as standard.
-
By one or two optional keylocks.
Keylocks can be used in addition to padlocks.
VSPD Chassis Locking by Keylock Accessory
The chassis locking by keylock accessory and the locking and unlocking procedures are the same as for the chassis locking in disconnected position.
Adapting the Chassis
DANGER |
|---|
|
HAZARD OF DEVICE FALLING
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGE
The chassis must be securely fastened when installing
or removing the device.
Failure to follow these instructions can result in equipment damage.
|
Follow this procedure to adapt the chassis locking mechanism so that the chassis can be locked in any position.
|
Stage |
Description |
|---|---|
|
1 |
Removing the terminal block identification plate and the chassis front cover. (Refer to the following procedure) |
|
2 |
|
|
3 |
Reinstalling the chassis front cover and the terminal block identification plate. |
Removing the Terminal Block Identification Plate and the Chassis Front Cover
Before starting the procedure, check that the circuit breaker is in the disconnected position and remove the circuit breaker from the chassis.
DANGER