DOCA0284EN-04

Circuit Breaker Locking Actions

About Locking Actions

@experts: Content shared between DOCA0284 and DOCA0285, with profiling; indicate if comments do not apply to both guides

A locking action is a manual locking operation made by the user. A number of optional locking accessories are available for the MasterPacT MTZ1 circuit breaker and chassis. For a complete listing of available locks, refer to LVPED225010EN MasterPacT MTZ with MicroLogic Active Control Unit - Catalog in Related Documents at the beginning of this guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?