DOCA0284EN-04

Go2SE Landing Page

@TW: topic shared between DOCA0265, DOCA0284 and DOCA0285

Presentation

When the QR code on the front face of a MasterPacT MTZ circuit breaker is scanned with a smartphone running a QR code reader and connected to the Internet, the Go2SE landing page is displayed.

The landing page displays:

  • Information about the MicroLogic Active control unit, including traceability information.

  • Zigbee ID and installation code for MicroLogic Active AP/EP control unit.

  • A list of menus.

Landing Page Description

The landing page is accessible from Android and iOS smartphones. It displays the same list of menus with slight differences in presentation.

The landing page shows:

  • Product image

  • Links to Register Product

  • Overview

    • Serial number

    • Reference

    • Description

  • Resource Center

    • Access all documents

      • Instruction sheets

      • User guides

      • Brochures

      • Declarations of conformity

    • Access to documents sorted by usage:

      • Install

      • Operate

      • Maintain

      • Monitor

      • Cybersecurity

    • Environmental data

    • Spare Parts

  • Support

Serial Number

The serial number provides traceability by encoding the manufacturing date and location of the MicroLogic Active control unit.

Zigbee ID and Installation Code

TBC@Osman

Click on More details to get the Zigbee ID and installation code. If using selective discovery, the Zigbee ID is used to discover a MicroLogic Active AP/EP control unit with a Panel Server.

The Zigbee ID (IEEE address) is a hexadecimal number with 16 characters, for example 8C6FB9FFFEF7A574.

The installation code is a hexadecimal number with 36 characters, for example 1F4A547964BC254A1F4A547964BC254ABC12.

mySchneider App

Selecting this application gives access to the Schneider Electric customer care mobile application mySchneider app that can be downloaded on Android and iOS smartphones. For smartphone compatibility, check on your application store. The customer care application offers self-service instructions and easy access to expert support and information.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?