DOCA0105EN-10

EIFE Interface Specific Commands

Reset EIFE Alarms

To reset EIFE interface alarms, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

41099

Command code = 41099

0x1F40

8001

INT16U

10

Number of parameters (bytes) = 10

0x1F41

8002

INT16U

8705 (0x2201)

Destination = 8705 (0x2201)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

Preset Cradle/Drawer Counters

To preset the cradle or drawer counters, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

41352

Command code = 41352

0x1F40

8001

INT16U

16

Number of parameters (bytes) = 16

0x1F41

8002

INT16U

8705

Destination = 8705 (0x2201)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

0–65535

Connected counter reset/preset:

  • 0–65534 = preset value of the connected counter

  • 65535 (0xFFFF) = do not preset the connected counter

0x1F46

8007

INT16U

0–65535

Disconnected counter reset/preset:

  • 0–65534 = preset value of the disconnected counter

  • 65535 (0xFFFF) = do not preset the disconnected counter

0x1F47

8008

INT16U

0–65535

Test counter reset/preset:

  • 0–65534 = preset value of the test counter

  • 65535 (0xFFFF) = do not preset the test counter

Preset Regrease Timers

To preset regrease timers, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

41353

Command code = 41353

0x1F40

8001

INT16U

18

Number of parameters (bytes) = 18

0x1F41

8002

INT16U

8705

Destination = 8705 (0x2201)

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45–0x1F46

8006–8007

INT16U

Operating time since last grease maintenance

  • 0–157766400 = preset value of regrease timer counter

  • 4294967295 (0xFFFFFFFF) = No preset

0x1F47–0x1F48

8008–8009

 

INT32U

Operating time since last move in rack in position (delay from last disconnection)

  • 0–28944000 = preset value of remove timer

  • 4294967295 (0xFFFFFFFF) = No preset

Get Events Command

To get events, set the command registers in the following way:

Address

Register

Unit

Type

Range

Bit

Description

0x1F3F

8000

INT16U

50560

Command code = 50560

0x1F40

8001

INT16U

27

Number of parameters (bytes) = 27

0x1F41

8002

INT16U

8705 (0x2201)

Destination = 8705 (0x2201)

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–

0x1F44

8004–

8005

OCTET STRING

Password of the command = 0 (no password required)

0x1F45

8006

Reserved

0x1F46

8007

INT16U

0, 2

Requested get event method Get Events Procedure:

  • 0 = Most recent events

  • 2 = Events before and up to a sequence number

0x1F47–0x1F4A

8008–8011

Reserved

0x1F4B–0x1F4C

8012–8013

INT32U

Requested event sequence number (for method 2 only)

0x1F4D

8014

INT16U

Requested event severity

0–7

Reserved

8

Low

9

Medium

10

High

11–15

Reserved

Events are returned to command registers in the following way:

Address

Register

Unit

Type

Range

Bit

Description

0x1F53

8020

INT16U

50560

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

Number of bytes returned

0x1F56

8023

Reserved

0x1F57

8024

INT16U

0, 2

Responded event requested method:

  • 0 = Most recent events

  • 2 = Events before and up to a sequence number

0x1F5E

8031

INT16U

Responded event severity

0–7

Reserved

8

Low

9

Medium

10

High

11–15

Reserved

0x1F5F

8032

INT16U

MSB: Number of events returned

LSB: Remaining events

  • 0 = No more events to get

  • 1 = More events to get

0x1F60

8033

INT16U

1013-25630

First event code

0x1F61–0x1F64

8034–8037

DATETIME

Timestamp of the first event

0x1F65

8038

INT16U

Timestamp quality of the first event

0x1F66–0x1F67

8039–8040

INT32U

First event sequence number

0x1F68

8041

INT16U

MSB: First event status

  • 1 = Occurrence

  • 2 = Completion

  • 3 = Pulse

LSB: Reserved

0x1F69

8042

Reserved

0x1F6A

8043

INT16U

First event severity

0–7

Reserved

8

Low

9

Medium

10

High

11–15

Reserved

0x1F6B–0x1F75

8044–8054

INT16U

Characteristics of event 2 (same as event 1)

0x1F76–0x1F80

8055–8065

INT16U

Characteristics of event 3 (same as event 1)

0x1F81– 0x1F8B

8066–8076

INT16U

Characteristics of event 4 (same as event 1)

0x1F8C–0x1F96

8077–8087

INT16U

Characteristics of event 5 (same as event 1)

0x1F97–0x1FA1

8088–8098

INT16U

Characteristics of event 6 (same as event 1)

0x1FA2–0x1FAC

8099–8109

INT16U

Characteristics of event 7 (same as event 1)

0x1FAD–0x1FB7

8110–8120

INT16U

Characteristics of event 8 (same as event 1)

0x1FB8–0x1FC2

8121–8131

INT16U

Characteristics of event 9 (same as event 1)

0x1FC3–0x1FCD

8132–8142

INT16U

Characteristics of event 10 (same as event 1)

Get Events Procedure

The command allows to get events by using one of the two following methods:

  • get the most recent events

  • get events before and up to an event sequence number. The event sequence number is an event identifier defined by the device, and is available among the event characteristics. It can be used to sort the events in chronological order.

The command allows to get 10 events maximum for one or several severity levels.

  • To get the 10 most recent events, use the method “get the most recent events”.

  • If there are more than 10 events, use the other method “get events before and up to an event sequence number” to get rest of the events.

Example: Read all events

The following diagram shows the steps to follow to read all events recorded in the device:

EIFE Interface Events

Event Code

Description

2304

(0x0900)

Cradle position discrepancy

2305

(0x0901)

Cradle connected contact change

2306

(0x0902)

Cradle disconnected contact change

2307

(0x0903)

Cradle test contact change

2308

(0x0904)

Remove device from cradle and put it back

2309

(0x0905)

Cradle has reached its maximum number of operations

2310

(0x0906)

Remaining service life of cradle is below alarm threshold

2311

(0x0907)

New MicroLogic control unit has been detected

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?