DOCA0105EN-10

EIFE Interface Specific Registers

Cradle Alarms

Address

Register

RW

Unit

Type

Range

Bit

Description

0x3997

14744

R

INT16U

Quality of each bit of register 14745:

  • 0 = Invalid

  • 1 = Valid

0x3998

14745

R

INT16U

Cradle management alarms register

0

Cradle position discrepancy

1

No racking-out operation for the last 11 months

2

Cradle has reached its max number of operation

3

Remaining service life of cradle is below alarm threshold

4

New MicroLogic control unit has been detected

5–15

Reserved

Cradle Management

The table describes the registers related to the Cradle management function performed by EIFE embedded Ethernet interface.

Address

Register

RW

Unit

Type

Range

Bit

Description

0x3BC3

15300

R-RC

INT16U

Quality of each bit of register 15301:

  • 0 = Invalid

  • 1 = Valid

0x3BC4

15301

R-RC

INT16U

Cradle status

0–7

Reserved

8

Device in disconnected position (CD)

9

Device in connected position (CE)

10

Device in the test position (CT)

11–15

Reserved

0x3BC5–0x3BC6

15302–15303

R-RC-WC

INT32U

0–65534

Cradle connected position counter

This counter increments for each rising edge of the cradle connected position

0x3BC7–0x3BC8

15304–15305

R-RC-WC

INT32U

0–65534

Cradle disconnected position counter

This counter increments for each rising edge of the cradle disconnected position

0x3BC9–0x3BCA

15306–15307

R-RC-WC

INT32U

0–65534

Cradle test position counter

This counter increments for each rising edge of the cradle test position

0x3BCB–0x3BCE

15308–15311

R-RC

DATETIME

Timestamp of the last change for the cradle connected position

0x3BCF–0x3BD2

15312–15315

R-RC

DATETIME

Timestamp of the last change for the cradle disconnected position

0x3BD3–0x3BD6

15316–15319

R-RC

DATETIME

Timestamp of the last change for the cradle test position

0x3BD7–0x3BD8

15320–15321

R-WC

INT32U

Operating time since last grease maintenance

0x3BD9–0x3BDA

15322–15323

R-WC

INT32U

Operating time since last move connected position

0x3BDB

15324

R

INT16U

0-65534

Cradle contact regrease counter

0x3BDC–0x3BE0

15325–15329

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?