DOCA0105EN-10

Protection Set Commands without Session

List of Commands

The following table lists the protection set commands without session, their corresponding command codes, and user profiles:

Command

Command code

User profile

Set external neutral current transformer settings Set External Neutral Current Transformer Settings

45704

Administrator

Set external neutral voltage sensor settings Set External Neutral Voltage Sensor Settings

46472

Administrator

Set ZSI configuration parameters Set ZSI Configuration Parameter

49033

Administrator

Select active curve Select Active Curve

49545

Administrator or Operator

Set earth leakage alarm settings Set Earth Leakage Alarm Settings

51592

Administrator

Set ground fault alarm settings Set Ground Fault Alarm Settings

51599

Administrator

Set External Neutral Current Transformer Settings

To set the external neutral current transformer settings, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

45704

Requested command code

0x1F40

8001

INT16U

12

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

0–1

External neutral current transformer:

  • 0 = Not available

  • 1 = Available

Set External Neutral Voltage Sensor Settings

To set the external neutral voltage sensor settings, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

46472

Requested command code

0x1F40

8001

INT16U

12

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45

8006

 

INT16U

0–1

External neutral voltage sensor

  • 0 = Not available

  • 1 = Available

Set ZSI Configuration Parameter

To get the ZSI configuration parameters, use the get ZSI configuration parameters command Get ZSI Configuration Parameter.

To set the ZSI configuration parameter settings, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

49033

Requested command code

0x1F40

8001

INT16U

14

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45

8006

INT16U

MSB: ZSI configuration mode

  • 0 = Off

  • 1 = On

LSB: 0

0x1F46

8007

INT16U

0-2

ZSI protection selection

  • 0 = Short time

  • 1 = Ground fault/Earth fault

  • 2 = All

Select Active Curve

To get the active setting group, use the get active setting group command Get Active Setting Group.

To set the active setting group, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

49545

Requested command code

0x1F40

8001

INT16U

12

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator or Operator user profile password

0x1F45

8006

INT16U

MSB: Active setting group

  • 1 = Setting curve A

  • 2 = Setting curve B

LSB: Dual setting operating behavior

  • 0 = Local

  • 1 = IO module (1 wire)

  • 2 = IO module (2 wires)

  • 3 = Remote

NOTE: After selecting the active setting group, use the get active setting group command Get Active Setting Group to get the confirmation that the set command has been executed successfully.

Set Earth Leakage Alarm Settings

To get the earth leakage alarm settings, use the get earth leakage alarm settings command Get Earth Leakage Alarm Settings.

To set the earth leakage alarm settings, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

51592

Requested command code

0x1F40

8001

INT16U

24

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45–0x1F46

8006–8007

INT32U

0xFFFFFFFF

Reserved

0x1F47

8008

INT16U

MSB: Earth leakage alarm mode

  • 0 = Off (alarm disabled)

  • 1 = On (alarm enabled)

LSB: 0

0x1F48–0x1F49

8009–8010

A

FLOAT32

0.5–22.0 (step 0.1)

Earth leakage alarm threshold

0x1F4A–0x1F4B

8011–8012

s

FLOAT32

1-10

Earth leakage alarm time delay

Set Ground Fault Alarm Settings

To get the ground fault alarm settings, use the get ground fault alarm settings command Get Ground Fault Alarm Settings.

To set the ground fault alarm settings, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

51599

Requested command code

0x1F40

8001

INT16U

24

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45–0x1F46

8006–8007

INT32U

0xFFFFFFFF

Reserved

0x1F47

8008

INT16U

MSB: Ground fault alarm mode

  • 0 = Off (alarm disabled)

  • 1 = On (alarm enabled)

LSB: 0

0x1F48–0x1F49

8009–8010

A

FLOAT32

120–1200

Ground fault alarm threshold

0x1F4A–0x1F4B

8011–8012

s

FLOAT32

1-10

Ground fault alarm time delay

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?