DOCA0105EN-10

Password Management

General Description

FYI, this map is shared with MTZ Modbus Communication, Masterpact NT/NW Modbus, and Compact NSX Modbus communication guides.

Remote access to data on MicroLogic control units and the ULP modules of the IMU is protected by password. Remote access includes:

  • EcoStruxure Power Commission software

  • The communication network

  • EcoStruxure Power Device App

  • FDM128 display

  • IFE/EIFE webpages

The following four profiles are defined for remote access. Each IMU has a different password for each user profile.

  • Administrator

  • Services

  • Engineer

  • Operator

The Administrator password is required to write the settings to the MicroLogic control unit and the ULP modules of the IMU using the EcoStruxure Power Commission Software.

Each intrusive command via the command interface is assigned to one or several user profiles, and protected by the corresponding user profile password. The password for each intrusive command is indicated in the description of the command.

No password is required for non-intrusive commands through the command interface.

Default Passwords

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The default password for each user profile is as follows:

User profile

Default password

Administrator

‘0000’ = 0x30303030

Services

‘1111’ = 0x31313131

Engineer

‘2222’ = 0x32323232

Operator

‘3333’ = 0x33333333

Changing a Password

A password can be changed with the EcoStruxure Power Commission software.

Entering the current password for a given user profile is required to change the password of this user profile. Entering the Administrator password enables you to change the password of any user profile.

A password is composed of exactly 4 ASCII characters. It is case-sensitive and the allowed characters are:

  • Digits from 0 to 9

  • Letters from a to z

  • Letters from A to Z

Passwords of the IMU

The MicroLogic control unit and the ULP modules of the IMU must be protected by the same passwords for each user profile.

When using EcoStruxure Power Commission software to modify a password, the password gets modified in the MicroLogic control unit and the ULP modules of the IMU.

It is compulsory to assign the current IMU passwords to the new module in the IMU, in case of:

  • addition of a new ULP module in the IMU.

  • replacement of the MicroLogic control unit or one of the ULP module of the IMU.

Use EcoStruxure Power Commission software to modify the passwords of the new module to the current IMU passwords.

Example: Addition of an IO module in an IMU with a MicroLogic control unit and an IFE interface.

  • The IMU has user-defined passwords for each user profile.

  • The IO module has the default passwords for each user profile.

Use EcoStruxure Power Commission software to replace the default passwords of the IO module by the user-defined passwords of the IMU for each user profile.

Password Reset

In case that the Administrator password of the (IMU) is lost or forgotten, the password can be reset to the default password with EcoStruxure Power Commission software and the support of the Schneider Electric Customer Care Center.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?