DOCA0105EN-10

Protection Get Commands without Session

List of Commands

The following table lists the protection get commands without session, their corresponding command codes, and user profiles:

Command

Command code

User profile

Get neutral protection settings Get Neutral Protection Settings

51589

No password required

Get ZSI configuration parameters Get ZSI Configuration Parameter

49025

No password required

Get dual settings control configuration Get Dual Settings Control Configuration

49536

No password required

Get active setting group Get Active Setting Group

49537

No password required

Get ground fault alarm settings Get Ground Fault Alarm Settings

51590

No password required

Get earth leakage alarm settings Get Earth Leakage Alarm Settings

51591

No password required

Get Neutral Protection Settings

To get the neutral protection settings, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

51589

Requested command code

0x1F40

8001

INT16U

14

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

0x1F45–0x1F46

8006–8007

INT32U

0xFFFFFFFF

Key for the protection get command without session

The neutral protection settings are returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

51589

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

32

Number of bytes returned

0x1F56–0x1F57

8023–8024

INT32U

0xFFFFFFFF

Key for the protection get command without session

0x1F58

8025

INT16U

MSB: Neutral protection mode

  • 0 = Off

  • 1 = On

LSB: Neutral protection function supported

  • 0 = Not supported

  • 1 = Supported

0x1F59–0x1F5C

8026–8029

DATETIME

Timestamp of last change of neutral protection mode

0x1F5D

8030

INT16U

Timestamp quality of last change of neutral protection mode

0x1F5E–0x1F61

8031–8034

DATETIME

Timestamp of last change of any parameter of the neutral protection function

0x1F62

8035

INT16U

Timestamp quality of last change of any parameter of the neutral protection function

0x1F63

8036

INT16U

0–3

MSB: 0

LSB: Neutral protection type

  • 0 = OFF

  • 1 = 0.5

  • 2 = 1.0

  • 3 = Oversized

0x1F64–0x1F65

8037–8038

A

FLOAT32

Long time over current protection threshold

Get ZSI Configuration Parameter

To get the ZSI configuration parameter settings, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

49025

Requested command code

0x1F40

8001

INT16U

10

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

The ZSI configuration parameter settings are returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

49025

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

24

Number of bytes returned

0x1F56

8023

INT16U

MSB: ZSI configuration mode:

  • 0 = Off

  • 1 = On (tripping)

LSB: ZSI configuration function supported

  • 0 = Not supported

  • 1 = Supported

0x1F57–0x1F5A

8024–8027

DATETIME

Timestamp of last change of ZSI configuration mode

0x1F5B

8028

INT16U

Timestamp quality of last change of ZSI configuration mode.

0x1F5C–0x1F5F

8029–8032

DATETIME

Timestamp of last change of any parameter of the ZSI configuration

0x1F60

8033

INT16U

Timestamp quality of last change of any parameter of the ZSI configuration

0x1F61

8034

INT16U

0-2

ZSI protection selection:

  • 0 = Short time

  • 1 = Ground/Earth leakage

  • 2 = All

Get Dual Settings Control Configuration

To get the dual settings control configuration, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

49536

Requested command code

0x1F40

8001

INT16U

10

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

The dual settings control configuration are returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

49536

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

6

Number of bytes returned

0x1F56

8023

INT16U

MSB: Setting group control block mode (Dual settings mode)

  • 0 = Disabled (factory setting)

  • 1 = Enabled

LSB: Setting group control block operating behavior (Dual settings switch mode)

  • 0 = Local HMI

  • 1 = IO module (1 wire)

  • 2 = IO module (2 wires)

  • 3 = Remote

0x1F57–0x1F58

8024–8025

Reserved

Get Active Setting Group

To get the active setting group, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

49537

Requested command code

0x1F40

8001

INT16U

10

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

The active setting group is returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

49537

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

12

Number of bytes returned

0x1F56

8023

INT16U

MSB: Active setting group validation

  • 0 = Invalid, the selection of the active setting group is in progress

  • 1 = Valid

LSB: Active setting group

  • 1 = Setting group A

  • 2 = Setting group B

0x1F57–0x1F5A

8024–8027

DATETIME

Timestamp of last active setting group change

0x1F5B

8028

INT16U

Timestamp quality of last active setting group change

Get Ground Fault Alarm Settings

To set the ground fault alarm, use the set ground fault alarm settings command Set Ground Fault Alarm Settings.

To get the ground fault alarm settings, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

51590

Requested command code

0x1F40

8001

INT16U

14

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

0x1F45–0x1F46

8006–8007

INT32U

0xFFFFFFFF

Reserved

The ground fault alarm settings are returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F52

8020

INT16U

51590

Last command code

0x1F53

8021

INT16U

Command status:

0x1F54

8022

INT16U

34

Number of bytes returned

0x1F55–0x1F56

8023–8024

0xFFFFFFFF

Reserved

0x1F57

8025

INT16U

MSB: Ground fault alarm mode

  • 0 = Off

  • 1 = On

LSB: Ground fault alarm function supported

  • 0 = Not supported

  • 1 = Supported

0x1F58–0x1F61

8026–8035

Reserved

0x1F62–0x1F63

8036–8037

A

FLOAT32

120–1200

Ig alarm pickup value

0x1F64–0x1F65

8038–8039

s

FLOAT32

1–10

tg alarm time delay

Get Earth Leakage Alarm Settings

To set the earth leakage alarm, use the set earth leakage alarm settings command Set Earth Leakage Alarm Settings.

To get the earth leakage alarm settings, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

51591

Requested command code

0x1F40

8001

INT16U

14

Number of parameters of the command

0x1F41

8002

INT16U

5377 (0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

0x1F45–0x1F46

8006–8007

0xFFFFFFFF

Reserved

The earth leakage alarm settings are returned to command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

51591

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

34

Number of bytes returned

0x1F56–0x1F57

8023–8024

0xFFFFFFFF

Reserved

0x1F58

8025

INT16U

MSB: Earth leakage alarm mode

  • 0 =Off

  • 1 = On

LSB: Earth leakage alarm function supported

  • 0 = Not supported

  • 1 = Supported

0x1F59–0x1F62

8026–8035

Reserved

0x1F63–0x1F64

8036–8037

A

FLOAT32

0.5-22

Earth leakage alarm threshold

0x1F65–0x1F66

8038–8039

s

FLOAT32

1-10

Earth leakage alarm time delay

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?