DOCA0105EN-10

Standard Dataset

Description

FYI, this map is shared with NT/NW Modbus guide, NSX Modbus guide, MTZ Modbus guide

The standard dataset contains the most useful information of each IMU module in one convenient table. The standard dataset is available in the registers 32000 to 32341. It can be read with three read requests.

Each IMU module updates the values in the dataset registers on a regular basis.

The response time of requests to standard dataset registers is shorter than the response time of requests to device registers. Therefore, it is recommended to read the standard dataset registers instead of device registers, to improve the overall performance of the system Modbus Programming Recommendations.

The standard dataset can be used with:

  • the IFE Ethernet interface for one circuit breaker

  • the IFE Ethernet switchboard server

  • the EIFE embedded Ethernet interface for MasterPact MTZ drawout circuit breaker

  • the IFM Modbus-SL interface for one circuit breaker with part number LV434000

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?