Circuit Breaker Characteristics
System Settings
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x1FD8–0x1FD9 |
8153–8154 |
R |
V |
FLOAT32 |
208–1000 |
Rated voltage |
|
0x1FDA–0x1FDB |
8155–8156 |
R |
A |
FLOAT32 |
100–8000 |
Rated current |
|
0x1FDC |
8157 |
– |
– |
– |
– |
Reserved |
|
0x1FDD |
8158 |
R |
– |
INT16U |
0–1 |
Rated frequency:
|
|
0x1FDE–0x1FE0 |
8159–8161 |
– |
– |
– |
– |
Reserved |
|
0x1FE1 |
8162 |
R |
– |
INT16U |
0–1 |
Number of poles:
|
|
0x1FE2 |
8163 |
R |
– |
INT16U |
30–41 |
System type (see detailed description below):
|
|
0x1FE3–0x1FE4 |
8164–8165 |
R |
V |
FLOAT32 |
1000–1250 |
VT primary voltage |
|
0x1FE5–0x1FE6 |
8166–8167 |
R |
V |
FLOAT32 |
100–690 |
VT secondary voltage |
|
0x1FE7–0x1FEA |
8168–8171 |
R |
– |
DATETIME |
– |
Current date/time of the source. |
System type detailed description:
|
If... |
Then... |
Result |
|---|---|---|
|
the system is 3-pole circuit breaker with external neutral current transformer and without external neutral voltage tap |
system type = 30 |
|
|
the system is 3-pole circuit breaker without external neutral current transformer and without external neutral voltage tap |
system type = 31 |
|
|
the system is 3-pole circuit breaker without external neutral current transformer and with external neutral voltage tap |
system type = 40 |
|
|
the system is 3-pole circuit breaker with external neutral current transformer and external neutral voltage tap, or if the system type is 4-pole circuit breaker |
system type = 41 |
|
Hardware Revision
The hardware revision is an ASCII string using the format XXX.YYY.ZZZ with:
-
XXX = major version (000–127)
-
YYY = minor version (000–255)
-
ZZZ = revision number (000–255)
The NULL character ends the revision number.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2047–0x204C |
8264–8269 |
R |
– |
OCTET STRING |
– |
Hardware revision |
Protection Type
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x204E |
8271 |
R |
– |
INT16U |
– |
Protection type:
|
Application Type
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x204F |
8272 |
R |
– |
INT16U |
1 |
Application type:
|
Circuit Breaker Standard
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2072 |
8307 |
R |
– |
INT16U |
0–3 |
Standard or market targeted by the device:
|
Firmware Revision
The firmware revision is an ASCII string using the format XXX.YYY.ZZZ with:
-
XXX = major version (000–127)
-
YYY = minor version (000–255)
-
ZZZ = revision number (000–255)
The NULL character ends the revision number.
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x2094-0x2099 |
8341–8346 |
R |
– |
OCTET STRING |
– |
Firmware revision |
Measurement Settings
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x20C9 |
8394 |
R |
– |
INT16U |
– |
Current demand calculation:
|
|
0x20CA–0x20CB |
8395–8396 |
R-WC |
min |
FLOAT32 |
– |
Current demand calculation interval time |
|
0x20CC |
8397 |
– |
– |
– |
– |
Reserved |
|
0x20CD |
8398 |
R |
– |
INT16U |
– |
Power demand calculation:
|
|
0x20CE–0x20CF |
8399–8400 |
R-WC |
min |
FLOAT32 |
– |
Power demand calculation interval time |
|
0x20D0 |
8401 |
– |
– |
– |
– |
Reserved |
|
0x20D1 |
8402 |
R-WC |
– |
INT16U |
0–1 |
External neutral voltage sensor:
|
|
0x20D2 |
8403 |
R-WC |
– |
INT16U |
0–1 |
External neutral current sensor:
|
|
0x20D3 |
8404 |
R-WC |
– |
INT16U |
0, 2 |
Power factor sign convention:
|
|
0x20D4 |
8405 |
R-WC |
– |
INT16U |
0–1 |
Power sign:
|
|
0x20D5 |
8406 |
– |
– |
– |
– |
Reserved |
|
0x20D6 |
8407 |
R-WC |
– |
INT16U |
0–1 |
Energy accumulation mode:
|
|
0x20D7 |
8408 |
R |
– |
INT16U |
0–1 |
Power calculation method:
|
Device Identification
|
Address |
Register |
RW |
Unit |
Type |
Range |
Description |
|---|---|---|---|---|---|---|
|
0x20D9 |
8410 |
R |
– |
INT16U |
– |
Internal identifier of the product:
|
|
0x20DA–0x20E3 |
8411–8420 |
R |
– |
OCTET STRING |
– |
Vendor name: ‘Schneider Electric’ |
|
0x20E4–0x2123 |
8421–8484 |
R |
– |
OCTET STRING |
– |
Vendor URL |
|
0x2124–0x212D |
8485–8492 |
R |
– |
OCTET STRING |
– |
Product range: ‘ MicroLogic ’ |
|
0x212C–0x2132 |
8493–8500 |
R |
– |
OCTET STRING |
– |
Product model |
|
0x2134–0x213B |
8501–8508 |
R |
– |
OCTET STRING |
– |
Product code |
|
0x213C–0x2148 |
8509–8521 |
R |
– |
OCTET STRING |
– |
Serial number of the MicroLogic control unit |
|
0x2149–0x2168 |
8522–8553 |
R-WC |
– |
OCTET STRING |
– |
User application name |
|
0x2169–0x2178 |
8554–8569 |
R |
– |
OCTET STRING |
– |
Main capability of device |
|
0x2179 |
8570 |
– |
– |
– |
– |
Reserved |
|
0x217A–0x2181 |
8571–8578 |
R |
– |
OCTET STRING |
– |
Product range: ‘ MasterPact MTZ ’ |
|
0x2182–0x2189 |
8579–8586 |
– |
– |
– |
– |
Reserved |
|
0x218A–0x218D |
8587–8590 |
R |
– |
OCTET STRING |
– |
Performance level:
|
|
0x218E–0x219A |
8591–8603 |
R |
– |
OCTET STRING |
– |
Serial number of the MasterPact MTZ circuit breaker |
|
0x219B–0x21AA |
8604–8619 |
R |
– |
OCTET STRING |
– |
Device family: ‘Circuit breaker’ |
Wireless Inhibition Status
|
Address |
Register |
RW |
Unit |
Type |
Range |
Bit |
Description |
|---|---|---|---|---|---|---|---|
|
0x887C |
34941 |
R |
– |
INT16U |
– |
– |
Quality of each bit of register 34942:
|
|
0x887D |
34942 |
R |
– |
INT16U |
– |
0 |
Bluetooth wireless inhibition status
|
|
1–15 |
Reserved |