DOCA0105EN-10

Session Management Commands

List of Commands

The following table lists the commands necessary to manage the editing session of the setting protection function in accordance with UL489SE standard, their corresponding command codes and user profiles.

Command

Command Code

User profile

Open setup session Open Setup Session

1930

Administrator

Apply settings Apply Settings

1932

Administrator

Get apply setting status Get Apply Setting Status

1924

No password required

Close setup session Close Setup Session

1933

Administrator

Open Setup Session

To open setup session, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

1930

Requested command code

0x1F40

8001

INT16U

10

Number of parameters of the command

0x1F41

8002

INT16U

5377

(0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

The session key for the editing session is returned to the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8020

INT16U

1930

Last command code

0x1F40

8021

INT16U

Command status:

0x1F41

8022

INT16U

4

Number of bytes returned

0x1F42–0x1F43

8023–8024

INT32U

0–4294967294

Session key for the command

Apply Settings

To apply settings, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

1932

Requested command code

0x1F40

8001

INT16U

14

Number of parameters of the command

0x1F41

8002

INT16U

5377

(0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45–0x1F46

8006–8007

INT32U

0–4294967294

Requested session key for the command

Get Apply Setting Status

To get apply setting status, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

1924

Requested command code

0x1F40

8001

INT16U

14

Number of parameters of the command

0x1F41

8002

INT16U

5377

(0x1501)

Destination of the command

0x1F42

8003

INT16U

0

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

0

Password of the command = 0 (no password required)

0x1F45–0x1F46

8006–8007

INT32U

0–4294967294

Requested session key for the command

The apply setting status is returned to the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F53

8020

INT16U

1924

Last command code

0x1F54

8021

INT16U

Command status:

0x1F55

8022

INT16U

6

Number of bytes returned

0x1F56–0x1F57

80023–8024

INT32U

0–4294967294

Responded session key for the command. It must be equal to the requested session key for the command.

0x1F58

8025

INT16U

0–1

Status of the apply settings command:

  • 0 = No apply settings in progress

  • 1 = Apply settings in progress

Close Setup Session

To close setup session, set the command registers in the following way:

Address

Register

Unit

Type

Range

Description

0x1F3F

8000

INT16U

1933

Requested command code

0x1F40

8001

INT16U

14

Number of parameters of the command

0x1F41

8002

INT16U

5377

(0x1501)

Destination of the command

0x1F42

8003

INT16U

1

Security type of the command

0x1F43–0x1F44

8004–8005

OCTET STRING

Password of the command: Administrator user profile password

0x1F45–0x1F46

8006–8007

INT32U

0–4294967294

Requested session key for the command

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?