DOCA0107EN-03

Factory Reset (6/7)

Overview

The Factory reset menu allows you to reset the following settings to factory values:

  • Alarm threshold

  • Alarm time delay

  • Pre-alarm threshold

  • Pre-alarm time delay

  • Alarm reset mode

  • Communication speed

  • Device address

  • Parity

Resetting to Factory Setting

Step

Action

1

Select Factory reset from the Home menu, and then press .

Result: Displays the Caution screen.

2

Press and enter the password to log in.

NOTE: If the password is incorrect, the password invalid screen is displayed and then, Caution screen is displayed.

3

After the login is successful, Confirmation screen is displayed.

Press within 10 seconds to confirm or abort.

NOTE: Press to cancel the factory reset. If you do not press any button within 10 seconds, the factory reset is cancelled automatically.

4

The settings are reset to factory value and the Information screen is displayed.

5

Press within 40 seconds to display the Home menu.

NOTE: The Metering screen displays if you:
  • press when settings are reset to factory value.

  • do not press any button within 40 seconds.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?