Test Menu (2/7)
Overview
The menu allows to test multiple functions of the VigiPacT RHU/RHUs relay:
-
The display lights up for a few seconds.
-
The indicators light up for a few seconds.
-
Channel measurement.
The two types of tests that can be performed are:
-
: It is a complete test with action on the pre-alarm and alarm outputs.
-
: It is a test with no action on the pre-alarm and alarm outputs.
A self-test can be performed:
-
Through menu on HMI.
-
Remotely through the Modbus network (only with VigiPacT RHU relay).
-
Remotely through output connectors (pins 25, 26).
-
resetting the maximum current value.
-
an alarm relay is active.
Testing Procedure
|
Step |
Action |
|---|---|
|
1 |
|
|
2 |
Select the required test sequence. |
|
3 |
|
|
4 |
At the end of test:
|