Settings Menu (3/7)
Overview
The menu displays the setting parameters.
The screen allows to set the following parameters:
-
: Alarm threshold
-
: Alarm time delay
-
: Pre-alarm threshold
-
: Pre-alarm delay
-
: Manual or Automatic
A password must be entered in the settings menu to modify the parameters.
Select the parameter to set and press
to display the parameter screen.
Functional Parameter Settings
|
Parameter |
Description |
|---|---|
|
Alarm threshold |
Where,
NOTE: After the validation of the new alarm threshold
value:
|
|
Alarm time delay |
Where,
NOTE:
|
|
Pre-alarm threshold |
Where,
NOTE:
|
|
Pre-alarm time delay |
Where,
NOTE: The values between 0 and 60 ms are prohibited
(the setting values are: 0, 60, 70 to 4500 ms).The pre-alarm time
delay will be set to alarm time delay value automatically if the pre-alarm
time delay is above the alarm time delay when the alarm threshold
and pre-alarm threshold are equal.
|
Alarm Reset Mode
The screen allows to select the alarm reset mode as Manual or Automatic.
The alarm reset can be configured through the HMI and Modbus (only for VigiPacT RHU relay).
If the alarm reset mode is Automatic, then the alarm is reset automatically.
If the alarm reset mode is Manual, you can reset the alarm manually through one of the following options:
-
by using a Reset button wired to the Reset input of the relay
-
by sending a reset command through Modbus communication (only for VigiPacT RHU relay)