DOCA0107EN-03

Metering Menu (1/7)

Overview

The Metering menu displays Metering and Maximum screens.

Metering Screen

The Metering screen displays the measured earth-leakage current (I) and the threshold current (IΔn). It also displays the earth-leakage current (I) metering in percentage with respect to the alarm threshold.

A

Measured earth-leakage current in mA from 10 mA to 999 mA (1 A to 60 A).

B

Measured earth-leakage current as percentage of alarm threshold value.

C

Display alarm threshold value in mA from 30 mA to 999 mA (1 A to 30 A).

Maximum Screen

The Maximum screen displays the maximum earth-leakage current detected by the device after the device is on.

A

Maximum measured earth-leakage current from 10 mA to 999 mA (1 A to 60 A).

B

Display alarm threshold value from 30 mA to 999 mA (1 A to 30 A).

Resetting the Maximum Measured Earth-Leakage Current

To reset the maximum measured earth-leakage current in the Maximum screen, press for 10 seconds and then release the button.

NOTE:
  • After is pressed for 5 seconds, the display starts blinking. If it is released after 5 seconds, the reset is cancelled.

  • The maximum measured earth-leakage current can be reset only in the Maximum screen.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?