Channel Summary Registers
Channel Status
|
Address |
Register |
RW |
Units |
Type |
Range |
Factory |
Saved |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x00C8 |
201 |
R |
NA |
BITMAP |
NA |
0x0001 |
No |
– |
Validity of each bit of alarm status: 0 = invalid 1 = valid |
|
0x00C9 |
202 |
R |
NA |
BITMAP |
NA |
0x0000 |
No |
Alarm status |
|
|
0 |
0 = no alarm 1 = alarm |
||||||||
|
1–15 |
Reserved |
||||||||
|
0x00CA |
203 |
R |
NA |
BITMAP |
NA |
0x0001 |
No |
– |
Validity of each bit of pre-alarm status: 0 = invalid 1 = valid |
|
0x00CB |
204 |
R |
NA |
BITMAP |
NA |
0x0000 |
No |
– |
Pre-alarm status |
|
0 |
0 = no pre-alarm 1 = pre-alarm |
||||||||
|
1–15 |
Reserved |
||||||||
|
0x00CC |
205 |
R |
NA |
BITMAP |
NA |
0x0001 |
No |
– |
Validity of each bit of alarm memorized: 0 = invalid 1 = valid |
|
0x00CD |
206 |
R |
NA |
BITMAP |
NA |
0x0000 |
Yes |
Alarm memorized |
|
|
0 |
0 = no alarm memorized 1 = alarm memorized |
||||||||
|
1–15 |
Reserved |
||||||||
|
0x00CE |
207 |
R |
NA |
BITMAP |
NA |
0x0001 |
No |
– |
Validity of each bit of toroid status: 0 = invalid 1 = valid |
|
0x00CF |
208 |
R |
NA |
BITMAP |
NA |
0x0000 |
No |
– |
Toroid status |
|
0 |
0 = no toroid connected 1 = toroid connected |
||||||||
|
1–15 |
Reserved |
||||||||
|
0x00CE |
209 |
RW |
NA |
INT16U |
NA |
0x0000 |
Yes |
Alarm reset mode 0 = manual 1 = automatic |
Measurements
|
Address |
Register |
RW |
Units |
Type |
Range |
Factory |
Saved |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0190 |
401 |
R |
mA |
INT16U |
0–60000 |
0x0000 |
No |
Measured earth-leakage current. |
|
0x01A4 |
421 |
R |
mA |
INT16U |
0–60000 |
0x0000 |
No |
Maximum of earth-leakage current measured. |
|
0x01B8 |
441 |
R |
NA |
INT16U |
0–200 |
0x0000 |
No |
Threshold percentage of measured earth-leakage current. |
Parameters
|
Address |
Register |
RW |
Units |
Type |
Range |
Factory |
Saved |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x01F4 |
501 |
RW |
mA |
INT16U |
30–30000 |
30 |
Yes |
Alarm threshold |
|
0x0200 |
513 |
RW |
ms |
INT16U |
0–4500 |
0 |
Yes |
Alarm trip delay |
|
0x020C |
525 |
RW |
mA |
INT16U |
15–30000 |
15 |
Yes |
Pre-alarm threshold |
|
0x0218 |
537 |
RW |
ms |
INT16U |
0–4500 |
0 |
Yes |
Pre-alarm trip delay |
Command Registers
|
Address |
Register |
RW |
Units |
Type |
Range |
Factory |
Saved |
Description |
|---|---|---|---|---|---|---|---|---|
|
0xEA76 |
60023 |
RW |
NA |
INT16U |
0–2 |
0x0000 |
Yes |
Allow to test the device.
|
|
0xEA77 |
60024 |
RW |
NA |
INT16U |
0–1 |
0x0000 |
Yes |
Alarm reset Bit 0 = 1: To reset the alarm |
|
0xEA78 |
60025(1) |
RW |
NA |
INT16U |
1–247 |
0x00F7 |
Yes |
Device Modbus address |
|
0xEA79 |
60026(1) |
RW |
NA |
INT16U |
0–3 |
0x0002 |
Yes(2) |
Communication speed setting
|
|
0xEA7A |
60027(1) |
RW |
NA |
INT16U |
0–2 |
0x0002 |
Yes(2) |
Communication parity setting
|
|
0xEA7B |
60028(1) |
RW |
NA |
INT16U |
0–1 |
0x0000 |
Yes |
|
|
(1) Communication may be broken if the parameter is modified. Communication has to be re-established with the new value written in the register. (2) Modifiable only if Autogo is not active. |
||||||||
Diagnostics Registers
|
Address |
Register |
RW |
Units |
Type |
Range |
Factory |
Saved |
Description |
|---|---|---|---|---|---|---|---|---|
|
0xEA7C |
60029 |
R |
NA |
INT16U |
0-0x0FFF |
0x0000 |
Yes |
Number of software resets. |
|
0xEA7D |
60030 |
R |
NA |
INT16U |
0-0x0FFF |
0x0000 |
Yes |
Number of times the device is powered on. |