DOCA0107EN-03

Communication Menu (4/7): for VigiPacT RHU Relay

Overview

The Communication settings menu allows to set the following parameters:

  • Device address

  • Communication speed

  • Parity

The figure displays the Communication settings menu.

Communication Parameters

Parameters

Authorized Value

Factory Value

Device address

1 to 247

247

Com speed

  • 4800

  • 9600

  • 19200

  • 38400

  • Auto

19200

Parity

  • None

  • Odd

  • Even

Even

NOTE: When the communication speed is set to Auto, the parity is not available because the parity is adapted automatically with the speed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?