DOCA0107EN-03

Integration of VigiPacT RHU Relay in Communication Architecture

Communication Architecture

A

FDM128 Ethernet display for eight devices

B

IFE Ethernet switchboard server

C

IFM Modbus-SL interface for one circuit breaker

D

VigiPacT RHU monitoring and protection relay

E

FDM121 ULP display for one circuit breaker

F

RJ45 male/male ULP cord

G

VigiPacT toroid

H

IO input/output application module for one circuit breaker

I

MasterPact NW circuit breaker

J

Circuit breaker BCP ULP cord

K

NSX cord

L

ComPacT NSX circuit breaker

M

Cable for Modbus SL-1x RJ45 and 1x Free wires

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?