Parameter Modification
Overview
To modify the value of a parameter, follow either of the methods described below:
-
Select a value in a list.
-
Modify a numerical value, digit by digit.
Selecting a Value in a List
To select a value, use the menu buttons as described below:
Modifying a Numerical Value
The numerical value of a parameter is made up of digits from 0 to 9.
To modify the numerical value, use the menu buttons as described below:
|
Icons |
Description |
|---|---|
|
Allows to increase the numerical value. |
|
|
Allows to decrease the numerical value. |
|
|
Allows to:
|
|
|
Allows to exit the current parameter entry. |
Pressing Multiple Buttons
If multiple buttons are pressed simultaneously, no action is performed and the pressed buttons are ignored except for the password reset function (refer to Password Management (7/7)). Release the pressed buttons to press another button.