Functional Description
Overview
The earth-fault protection consists of measuring the earth-leakage current in an electrical installation, and disconnecting the installation when the current becomes hazardous to life and property.
Functions
The VigiPacT RHU/RHUs relay is used together with a VigiPacT toroid (open or closed) or a rectangular sensor.
-
Measures the earth-leakage current detected by the toroid.
-
Displays the earth-leakage current.
-
Trips the installation protection circuit breaker through an MN or MX release if the earth-leakage current exceeds the threshold IΔN for a time greater than the delay Δt.
-
Implements two earth-leakage current thresholds, one corresponding to a pre-alarm and an other to an alarm.
-
Communicates via the Modbus communication serial line (only for VigiPacT RHU relay).
Alarm Detection
The alarm threshold I alarm corresponds to an earth-leakage current that is hazardous for the installation.
An alarm is active when the measured earth-leakage current is greater than the set alarm threshold (I alarm) on toroid for a period of time greater than the set alarm delay (t alarm in milliseconds or seconds).
-
When an alarm is active, the and LEDs are switched on.
-
When alarm is detected, the screen is displayed, and the earth-leakage current value blinks.
Pre-alarm Detection
The pre-alarm threshold I pre-alarm correspond to an earth-leakage level that must be eliminated before it becomes hazardous for the installation.
A pre-alarm is active when the measured earth-leakage current is greater than the set pre-alarm threshold for a period of time greater than the set pre-alarm trip delay (t pre-alarm in milliseconds or seconds).
-
When a pre-alarm is active, the LED is switched on.
-
When pre-alarm is detected, the screen is displayed and the earth-leakage current value blinks.