Channel Detailed Registers
Mapping of the Detailed Channel Register
|
Address |
Register |
|---|---|
|
0x03E8–0x03FB |
1001-1020 |
Status and Control Registers
|
Address |
Register |
RW |
Units |
Type |
Range |
Factory |
Saved |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x03E8 |
1001 |
R |
NA |
BITMAP |
NA |
0x003F |
No |
– |
Validity of each bit of Status:
|
|
0x03E9 |
1002 |
R |
NA |
BITMAP |
NA |
0x0000 |
No |
Channel 1 status |
|
|
0 |
Alarm |
||||||||
|
1 |
Pre-alarm |
||||||||
|
2 |
Alarm is memorized |
||||||||
|
3 |
Toroid is connected |
||||||||
|
4 |
Alarm relay is active |
||||||||
|
5 |
Pre-alarm relay is active |
||||||||
|
6–15 |
Reserved |
||||||||
|
0x03EA–0x03EB |
1003–1004 |
R |
NA |
– |
NA |
0x8000 |
No |
– |
Reserved |
Measurement Registers
|
Address |
Register |
RW |
Units |
Type |
Range |
Factory |
Saved |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x03EC |
1005 |
R |
mA |
INT16U |
0–60000 |
0x0000 |
No |
Measured earth-leakage current. |
|
0x03ED |
1006 |
R |
mA |
INT16U |
0–60000 |
0x0000 |
No |
Maximum of earth-leakage current measured |
|
0x03EE |
1007 |
R |
% |
INT16U |
0–200 |
0x0000 |
No |
Threshold percentage of measured earth-leakage current. |
Parameter Registers
|
Address |
Register |
RW |
Units |
Type |
Range |
Factory |
Saved |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x03EF |
1008 |
RW |
mA |
INT16U |
30–30000 |
30 |
Yes |
Alarm threshold |
|
0x03F0 |
1009 |
RW |
ms |
INT16U |
0–4500 |
0 |
Yes |
Alarm trip delay |
|
0x03F1 |
1010 |
RW |
mA |
INT16U |
15–30000 |
15 |
Yes |
Pre-alarm threshold |
|
0x03F2 |
1011 |
RW |
ms |
INT16U |
0–4500 |
0 |
Yes |
Pre-alarm trip delay |
|
0x03F3–0x03FB |
1012–1020 |
R |
– |
BITMAP |
– |
0x0000 |
No |
Reserved |