DOCA0107EN-03

Troubleshooting

Event

Diagnostics

Action

LED ON switch is off

No indication of power supply.

  • Check the power supply of the relay.

  • After verification, if the problem persists, replace the relay by a new one.

Toroid connection lost

Alarm LED: blinking

Alarm relay: active

  • Check the connection of the toroid to the relay.

  • After verification, if the problem persists, replace the toroid by a new one.

Toroid connection detected

If the alarm reset mode is Manual, press to acknowledge the information.

Alarm detected

Alarm LED: blinking

Alarm relay: active

If the alarm reset mode is Manual, press to reset the alarm and deactivate the relay.

Password not valid

  • Enter the right password.

  • Reset the password, if the password is lost.

Test failed

  • Do the factory reset of the relay.

  • After the factory reset, if the test fails, replace the relay by new one.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?