DUG_ITRV_LK-01

Activating the child Lock

The Child Lock helps to prevent children from operating the Thermostats. When the child lock is turned on, the Thermostats can be operated only using the app, but not manually. To access the child lock feature, you must first enable the individual Thermostat visibility in the Home page.
To turn on the Child Lock settings:
TIP: By turning on the child lock, the Thermostat does not turn off, it remains in its current state.
  1. On the Home page, tap All devices > iTRV.
  2. Tap Settings.
  3. Tap the toggle switch (A) to turn on the Child Lock settings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?