DUG_ITRV_LK-01

Pairing device manually

To pair the device manually:
NOTE: Remember to insert the batteries to power on the device.
  1. On the Home page, tap +.
  2. Tap and select the required Wiser Hub on the slide-up menu.
  3. Select an option to add the device (A):
    • Add Device with Install Code
    • Add Device without Install Code

    TIP: It is highly recommended to add the device with install code.
  4. To pair the device with install code, tap Add Device with Install Code to display the slide-up menu. Select any one of the options (B):
    • Scan Install Code - you can scan the device for the install code
    • Enter Install Code Manually - you can manually enter the install code from the device
    After pairing the device with install code, proceed to Step 6.

  5. To pair the device without install code, tap Add Device without Install Code.
  6. Turn and hold the cap in the “+” direction for a few seconds.
    The middle LED blinks green.
  7. In the app, select Middle LED blinking in green and tap Start configuration (C).

  8. After a few seconds, a solid green LED indicates that the device is successfully paired to the Gateway/Hub.
  9. After the device is added in the app, tap Done.
    NOTE:
    • Before you tap Done, you can select the room to assign the Thermostats. This creates a group to control the Thermostats, refer to Using the device.

    • Refer to Changing the device location to assign a room to the Thermostat, if you did not assign the room at Step 9.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.