DUG_ITRV_LK-01

LED indications

Normal use

State

User Interaction

+ LED

Center LED

– LED

Duration

Boost up

Turn the cap in the + direction

   

Solid for 5 seconds

Boost down

Turn the cap in the - direction

   

Solid for 5 seconds

Head calibration

State

User Interaction

+ LED

Center LED

– LED

Duration

Start up

Insert the batteries

Single quick flash

Opening the valve

Automatic upon inserting batteries OR Turn and hold the cap in + direction for 8 seconds (for changing batteries)

   

Solid until the valve is open

Ready to pair

The thermostat is ready to install when the valve is fully open (see above)

Red and Blue: flash for up to 5 minutes

Orange solid = not joined | Green solid = joined

Closing the valve

Turn and hold the cap in the – direction for 2 seconds

   

Solid until the valve is closed

Joining

Turn and hold the cap in the + direction for 3 seconds

   

Pulses for up to 2 minutes

Successful Joining

Pairing process begins

   

Solid for 5 seconds

Unsuccessful joining

If no network is found after 2 minutes

   

Flashes for 5 seconds

Error detection state

State

User Interaction

+ LED

Center LED

– LED

Duration

Low battery

     

Solid for 1 second (Repeated each hour)

Critical battery

     

Fast flash for 5 seconds (Repeated each minute)

No signal/network

     

Solid with fade-out after 2 seconds.

NOTE: In this event, the thermostat has not joined the wiser system and must either join the gateway or be re-installed.

Turn the cap in the “–” direction to start a boost

   

Fast flash for 5 seconds (Repeated)

Turn the cap in the “+” direction to start a boost

   

Fast flash for 5 seconds (Repeated)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?