DUG_ITRV_LK-01

Removing the device

Using the Wiser app, you can remove a device from the device list.
To remove a device:
NOTE: You can only remove the device by accessing each Thermostat control page.
  1. On the Home page, tap All devices > iTRV.
  2. Tap to display more details.
  3. Tap Remove and Factory Reset Device (A) and tap OK.

    TIP: On the Home page, tap and hold the iTRV to remove the device.
    NOTE: By removing the device, you will reset the device. If you still have a problem with the reset, then refer to reset the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?