DUG_ITRV_LK-01

Schedule actions within boost period

If the boost mode is turned on and in this period if there are one or more scheduled actions, the system stops the schedule action temporarily and only performs the boost operation until the boost duration is completed.

To view the temperature changes during the boost operation, go to Checking the device history.

Below is an example of the temperature changes during the boost duration:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?