DUG_ITRV_LK-01

Replacing the batteries

Replace the batteries when the battery is low or critically low. The center LED of the thermostat will signal when the batteries need to be replaced.
+ LED Centre LED – LED Meaning
Off Solid Red, for 1s, once per hour. Off Battery, low. Replace.
NOTE: This sends notification to the app.
Off Flashes Red, for 5s, once per minute. Off Batteries critically low.
Replace immediately.
NOTE: This sends notification to the app.

Replace the batteries with 2*1.5V IEC LR6 (AA) alkaline batteries. Check the batteries ("+" and "-" ends) are correctly oriented. The polarity is indicated on the device's terminals.

NOTE: Used batteries should be disposed of according to statutory regulations. They must be recycled properly which help to protect the environment and reduce the waste of precious resources.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?