DUG_ITRV_LK-01

When the current temperature is higher than setpoint

When the current temperature value is equal to or higher than the setpoint, the flame icon on the control panel page will be displayed in grey state (A).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?