DUG_ITRV_LK-01

Pairing device with auto scan

Pairing the device with auto scan automatically discovers the device when the corresponding device is powered on.
To pair the device:
NOTE: Remember to insert the batteries to power on the device.
  1. On the Home page, tap +.
  2. Tap Auto scan and tap Confirm.
  3. If you have multiple gateways, do Step 4 or proceed to Step 5.
  4. Tap Select hub and select the Wiser hub from the slide-up menu.
  5. Turn and hold the cap in the “+” direction for a few seconds.
    NOTE: Please wait for a few seconds until the device search is complete.
  6. Tap Next (A) and select iTRV.

  7. Once the device is added successfully, tap Done.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?