DUG_ITRV_LK-01

Resetting the device

You can reset the device to factory default manually while it is attached to the radiator body.
To reset the device:
  1. Turn and hold the cap in the “-” direction.
  2. Wait a few seconds until the center LED begins to flash Red.
  3. Continue holding the cap in “-” direction until LED flashes Red 8 times.
  4. Release the cap; all 3 LEDs will flash red-orange-blue once indicating successful reset of the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?